Trust GXT 833 Thado keyboard Gaming USB Spanish Black, Silver
Product code:
24067
Brand:
Trust
Product name:
GXT 833 Thado
GTIN (EAN/UPC):
8713439240672
Bullet Points Trust GXT 833 Thado keyboard Gaming USB Spanish Black, Silver:
- Compact TKL design (80%) takes up limited space on your desk or in your bag
- Multicolour LED lighting with breathing effect
- Anti-Ghosting: Up to 10 simultaneous key presses
- Sturdy metal backplate with anti-skid rubber feet for extra stability
- 12 direct access media keys
- Special gaming mode that disables the Windows key
- 1.8m braided cable
Warranty:
2 years
Long product name Trust GXT 833 Thado keyboard Gaming USB Spanish Black, Silver:
USB, LED, TKL, 1.5 m, ES, 359 x 135 x 40 mm
Trust GXT 833 Thado keyboard Gaming USB Spanish Black, Silver:
The Compact King
As a gamer, you only want the best hardware to ensure your road to victory. But if you like to take this hardware with you to LAN parties, tournaments or events, a smaller form factor might come in handy. The Trust GXT 833 Thado is a tenkeyless gaming keyboard, 20% smaller than keyboards with a numpad, making it easier to take with you. Its metal backplate makes the Thado sturdy, while the LED illumination lights up the party.
Tenkeyless design
The Thado has a tenkeyless design, which means it only takes up 80% of the space a keyboard with a full-size layout would. This is especially useful if you don’t have that much desk space or if you like to take your hardware with you on the go. But don’t be fooled by the smaller form factor. This TKL keyboard still does everything you’d come to expect from a gaming keyboard.
Feature Rich
The Trust Thado is jam-packed with features that put the gamer first. Like anti-ghosting, making sure you can press up to 10 buttons simultaneously. All of your commands will be registered by your game. The gaming mode will keep you in the game by disabling the Windows key, while the anti-skid rubber feet will keep this gaming keyboard in place, even during the most heated matches.
In Control
During your gaming sessions, you’re in complete control of any situation your opponent throws at you. But after you’re done, you’re just as in control when it comes to your media. The 12 direct access media keys make sure you’ve got full control over your music and videos.
Breathing Effect
Functionality is one thing, but don’t forget about the look! Thanks to the LED illumination of the Trust Thado TKL, you’ll be sure to outshine the competition in any situation. So take a good look at the breathing effect, focus on the task at hand and start winning those battle royals.
As a gamer, you only want the best hardware to ensure your road to victory. But if you like to take this hardware with you to LAN parties, tournaments or events, a smaller form factor might come in handy. The Trust GXT 833 Thado is a tenkeyless gaming keyboard, 20% smaller than keyboards with a numpad, making it easier to take with you. Its metal backplate makes the Thado sturdy, while the LED illumination lights up the party.
Tenkeyless design
The Thado has a tenkeyless design, which means it only takes up 80% of the space a keyboard with a full-size layout would. This is especially useful if you don’t have that much desk space or if you like to take your hardware with you on the go. But don’t be fooled by the smaller form factor. This TKL keyboard still does everything you’d come to expect from a gaming keyboard.
Feature Rich
The Trust Thado is jam-packed with features that put the gamer first. Like anti-ghosting, making sure you can press up to 10 buttons simultaneously. All of your commands will be registered by your game. The gaming mode will keep you in the game by disabling the Windows key, while the anti-skid rubber feet will keep this gaming keyboard in place, even during the most heated matches.
In Control
During your gaming sessions, you’re in complete control of any situation your opponent throws at you. But after you’re done, you’re just as in control when it comes to your media. The 12 direct access media keys make sure you’ve got full control over your music and videos.
Breathing Effect
Functionality is one thing, but don’t forget about the look! Thanks to the LED illumination of the Trust Thado TKL, you’ll be sure to outshine the competition in any situation. So take a good look at the breathing effect, focus on the task at hand and start winning those battle royals.