ADATA 1GB DDR3-1333MHz SO-DIMM memory module 1 x 1 GB 204-pin SO-DIMM
Product code:
AD3S1333B1G9-R
Brand:
ADATA
Product name:
1GB DDR3-1333MHz SO-DIMM
Bullet Points ADATA 1GB DDR3-1333MHz SO-DIMM memory module 1 x 1 GB 204-pin SO-DIMM:
- 1 GB DDR3
- 204-pin SO-DIMM 1 x 1 GB
- CAS latency: 9
- 1.5 V
Long product name ADATA 1GB DDR3-1333MHz SO-DIMM memory module 1 x 1 GB 204-pin SO-DIMM:
1GB DDR3-1333MHz SO-DIMM
ADATA 1GB DDR3-1333MHz SO-DIMM memory module 1 x 1 GB 204-pin SO-DIMM:
A-DATA DDR3 1333 Unbuffered SO-DIMM compliance with JEDEC standard specifications, with the original BGA package 128Mx8 particles to provide 1GB, 2GB capacity, such as options, with high stability demands the best choice as a PC.
DDR3 voltage of 1.5V in the design, which is lower than the work of the current-voltage DDR2 1.8V for the rate of consumption is expected to save 30%. The increasingly significant global environmental requirements, A-DATA also fully support low power consumption of DDR3 products . DDR3 clock to enhance the effectiveness of the performance, signal quality is relatively strict. product validation phase in the project, A-DATA Technology has set up a complete assessment of the testing so that products can be different from the stability of the industry.
DDR3 voltage of 1.5V in the design, which is lower than the work of the current-voltage DDR2 1.8V for the rate of consumption is expected to save 30%. The increasingly significant global environmental requirements, A-DATA also fully support low power consumption of DDR3 products . DDR3 clock to enhance the effectiveness of the performance, signal quality is relatively strict. product validation phase in the project, A-DATA Technology has set up a complete assessment of the testing so that products can be different from the stability of the industry.