StarTech.com Thunderbolt 3 to Thunderbolt 2 Adapter - TB3 Laptop to TB2 Displays & Devices - Thunderbolt 2 20Gbps or Thunderbolt 1 10Gbps Converter - Thunderbolt 3 Certified- Windows/Mac
Product code:
TBT3TBTADAP
Brand:
StarTech.com
Product name:
Thunderbolt 3 to Thunderbolt 2 Adapter - TB3 Laptop to TB2 Displays & Devices - Thunderbolt 2 20Gbps or Thunderbolt 1 10Gbps Converter - Thunderbolt 3 Certified- Windows/Mac
GTIN (EAN/UPC):
0065030864138, 065030864138, 5054629963555
Bullet Points StarTech.com Thunderbolt 3 to Thunderbolt 2 Adapter - TB3 Laptop to TB2 Displays & Devices - Thunderbolt 2 20Gbps or Thunderbolt 1 10Gbps Converter - Thunderbolt 3 Certified- Windows/Mac:
- COMPATIBILITY NOTE: This Thunderbolt 3 to Thunderbolt 2 adapter is NOT BIDIRECTIONAL and will not connect TB3 peripherals to computers with TB1/TB2 ports; This adapter is not compatible w/ Mini DisplayPort / DisplayPort monitors or Thunderbolt 4 computers
- THUNDERBOLT 3 TO THUNDERBOLT ADAPTER: Enables Thunderbolt 3 laptops to connect with older Thunderbolt 2 (20Gbps) and Thunderbolt 1 (10Gbps) peripherals; Connect TB1/TB2 devices like external storage drive bays, or Thunderbolt Displays to your TB3 laptop
- THUNDERBOLT 3 CERTIFIED: Compatible w/ TB3 certified laptops like MacBook Air & MacBook Pro, Dell XPS 13 & 15, Latitude, Precision, Lenovo ThinkPad X1, P series, HP EliteBook; Requires TB3 host (laptop or desktop must be equipped with Thunderbolt 3 port)
- TECH SPECS: Bus-powered; Provides up to 12W of power for peripherals; Features a physical Mini DisplayPort connector but it is not capable of adapting to mini DisplayPort / DisplayPort signal; Only compatible w/ Thunderbolt peripherals; 8in built-in cable
- COMPATIBLE WITH THUNDERBOLT DISPLAYS: This TB3 to TB2/TB1 adapter enables use of older Thunderbolt monitors (27" Apple Thunderbolt Displays/LG Ultrawide TB2 display) w/ certified Thunderbolt 3 laptops; Windows and macOS compatible
Warranty:
2 Years
Long product name StarTech.com Thunderbolt 3 to Thunderbolt 2 Adapter - TB3 Laptop to TB2 Displays & Devices - Thunderbolt 2 20Gbps or Thunderbolt 1 10Gbps Converter - Thunderbolt 3 Certified- Windows/Mac:
StarTech.com Thunderbolt 3 to Thunderbolt 2 Adapter (Non-Reversible) - TB3 Laptop to TB2 (20Gbps) or TB1 (10Gbps) Devices / Displays - Black - Windows/Mac (TBT3TBTADAP)
StarTech.com Thunderbolt 3 to Thunderbolt 2 Adapter - TB3 Laptop to TB2 Displays & Devices - Thunderbolt 2 20Gbps or Thunderbolt 1 10Gbps Converter - Thunderbolt 3 Certified- Windows/Mac:
Use first-generation Thunderbolt and Thunderbolt 2 devices with your new Thunderbolt 3 computer
With this adapter, you can connect Windows and Mac based Thunderbolt™ 3 computers to older Thunderbolt devices, such as external hard drives, Thunderbolt displays, and older Thunderbolt capable Mac computers.
Because this adapter is backward compatible, you can connect to first-generation Thunderbolt devices at 10Gbps speed. With Thunderbolt 2 devices, you can connect at 20Gbps. The adapter satisfies all requirements for bi-directional data transfers and simultaneous power for bus-powered devices.
The TBT3TBTADAP is backed by a 2-year warranty for guaranteed reliability.
This adapter is not compatible with Thunderbolt 4 computers
Your computer's Thunderbolt 3 ports might not function properly until you update one or more of the following on your computer:
• BIOS
• Thunderbolt firmware
• Thunderbolt 3 controller drivers
• Thunderbolt 3 software
The required updates will vary depending on your computer.
For an up-to-date list of affected computers and instructions, visit http://thunderbolttechnology.net/updates . If your manufacturer isn't listed on the Thunderbolt website, contact your manufacturer.
The StarTech.com Advantage
With this adapter, you can connect Windows and Mac based Thunderbolt™ 3 computers to older Thunderbolt devices, such as external hard drives, Thunderbolt displays, and older Thunderbolt capable Mac computers.
Because this adapter is backward compatible, you can connect to first-generation Thunderbolt devices at 10Gbps speed. With Thunderbolt 2 devices, you can connect at 20Gbps. The adapter satisfies all requirements for bi-directional data transfers and simultaneous power for bus-powered devices.
The TBT3TBTADAP is backed by a 2-year warranty for guaranteed reliability.
This adapter is not compatible with Thunderbolt 4 computers
Your computer's Thunderbolt 3 ports might not function properly until you update one or more of the following on your computer:
• BIOS
• Thunderbolt firmware
• Thunderbolt 3 controller drivers
• Thunderbolt 3 software
The required updates will vary depending on your computer.
For an up-to-date list of affected computers and instructions, visit http://thunderbolttechnology.net/updates . If your manufacturer isn't listed on the Thunderbolt website, contact your manufacturer.
The StarTech.com Advantage