Hercules INPULSE T7 PREMIUM Vinyl scratcher Black
Product code:
4780938
Brand:
Hercules
Product name:
INPULSE T7 PREMIUM
GTIN (EAN/UPC):
3362934746384
Bullet Points Hercules INPULSE T7 PREMIUM Vinyl scratcher Black:
- 2 motorized platters to practice DJing on vinyl
- Central mixer: genuine mixer layout
- Premium: gold-colored accents, built-in premium fader module, 1 carry bag and 2 extra felt slipmats for scratching included
Long product name Hercules INPULSE T7 PREMIUM Vinyl scratcher Black:
2 x XLR + 2 x RCA, 1/8” / 3.5 mm + 1/4” / 6.35, 44.1 kHz / 24-bit, 33 x 26 x 8.5 cm
Hercules INPULSE T7 PREMIUM Vinyl scratcher Black:
ueled by the success of its DJControl Inpulse range and the DJControl Inpulse T7, the DJControl Inpulse T7 Premium Edition comes with a range of unique enhancements and sleek finishes that will make it easier for modern DJs to scratch and perform anywhere. The controller features a high-quality premium fader module, two new slipmats ideal for scratching, two slipmats ideal for traditional mixing, a transport case and eye-catching gold details and markings.
Designed primarily to serve the hip-hop and scratching community that embraced the original DJControl T7 most enthusiastically, this new controller from Hercules will add a little extra heart to every beat.
The DJControl Inpulse T7 Premium Edition comes with two software licenses, Serato DJ Lite and DJUCED. It is compatible with Serato DJ Pro.
DJUCED AND SERATO COMPATIBILITY
To complete your DJ setup, you can connect your PC or Mac to the DJControl Inpulse T7 Premium and use free included DJ software like DJUCED or Serato DJ Lite. You can buy a licence or subscribe to the premium version of Serato DJ Pro if you want to improve your experience with it.
THE REAL DEAL
DJs wield the power to blend and beatmatch with precision, courtesy of the standard-sized 7" platters that leap from 0 to 33⅓ RPM in the blink of an eye. The magic doesn't stop there - they can even liberate the cherished vinyl discs and the velvety scratch slipmats from their metallic embrace, recreating an authentic turntable sensation in a digital format.
ENDLESS CREATIVITY
Stems – the magic, real-time audio separation tool that should be at the disposal of every DJ. With one-button controls to isolate vocals or instrumentals, DJs can easily create personalized mixes on the fly. There is truly no limit to the imagination when it comes to creating new mashups or blends. Available in DJUCED and Serato DJ.
POWERFUL FX FOR POWERFUL TRANSITIONS
Boasting a trio of FX Select buttons, a paddle, and a Filter knob per deck, along with an additional control knob and Beat -/+ buttons, the DJControl Inpulse T7 Premium provides users with the tools they need to fine-tune their mixes and transitions to perfection using a plethora of effects.
RELIABLE. PORTABLE. AND SO MUCH MORE
The DJControl Inpulse T7 Premium weighs only 11 lbs, so you can carry it with the included bag anywhere you go. It also comes with retractable feet so you can run wires underneath and protect your controller from spilled drinks. No more calling you DJ Backpain, promise.
BETTER, SMOOTHER MOVEMENT
Each fader on the included and already installed Premium Fader Module on the DJControl Inpulse T7 Premium slides on 2 rails for better, smoother movement than the stock faders on the DJControl Inpulse T7. The 3 double-rail faders are built to last, so you can focus on your music, not your equipment.
MAKING BACKSPINS YOUR REALITY
Placed between the motorized jogwheel platter and the vinyl record, the included Scratch Slipmats insulate the records from platter vibrations and allow you to handle the disc without affecting the platter’s rotation. The DJControl Inpulse T7 Premium also come with standard slipmats, ideal for traditional mixing.
TOTAL COMFORT, IN TOTAL STYLE
Lighter than hardened plastic, the semi-rigid EVA (Ethylene Vinyl Acetate) bag has a black lining featuring the Hercules logo embroidered in white and red. The EVA creates a solid shell which is softer than hardened plastic and won’t break on impact. Your controller and its power cables will fit into a foam cavity, making it safe to carry everywhere your DJ career takes you.
ALL THE AUDIO CONNECTIONS YOU NEED
The DJControl Inpulse T7 Premium, powered by a DC converter and connected to your laptop via USB, provides crucial master outputs (2 x XLR + 2 x RCA) for connecting to professional speaker systems. To meet your various audio needs, it also offers dual headphone connectivity options (1/8" / 3.5 mm stereo mini-jack + 1/4" / 6.35 mm stereo jack).
The controller has been honored with Magnetic Mag's Editors Choice Award 2023, recognized as the best new DJ turntables of the year. This prestigious award highlights the publication's top picks in production, audio, and DJ gear categories.
For more details, visit: Magnetic Mag Editors Choice Awards 2023
Designed primarily to serve the hip-hop and scratching community that embraced the original DJControl T7 most enthusiastically, this new controller from Hercules will add a little extra heart to every beat.
The DJControl Inpulse T7 Premium Edition comes with two software licenses, Serato DJ Lite and DJUCED. It is compatible with Serato DJ Pro.
DJUCED AND SERATO COMPATIBILITY
To complete your DJ setup, you can connect your PC or Mac to the DJControl Inpulse T7 Premium and use free included DJ software like DJUCED or Serato DJ Lite. You can buy a licence or subscribe to the premium version of Serato DJ Pro if you want to improve your experience with it.
THE REAL DEAL
DJs wield the power to blend and beatmatch with precision, courtesy of the standard-sized 7" platters that leap from 0 to 33⅓ RPM in the blink of an eye. The magic doesn't stop there - they can even liberate the cherished vinyl discs and the velvety scratch slipmats from their metallic embrace, recreating an authentic turntable sensation in a digital format.
ENDLESS CREATIVITY
Stems – the magic, real-time audio separation tool that should be at the disposal of every DJ. With one-button controls to isolate vocals or instrumentals, DJs can easily create personalized mixes on the fly. There is truly no limit to the imagination when it comes to creating new mashups or blends. Available in DJUCED and Serato DJ.
POWERFUL FX FOR POWERFUL TRANSITIONS
Boasting a trio of FX Select buttons, a paddle, and a Filter knob per deck, along with an additional control knob and Beat -/+ buttons, the DJControl Inpulse T7 Premium provides users with the tools they need to fine-tune their mixes and transitions to perfection using a plethora of effects.
RELIABLE. PORTABLE. AND SO MUCH MORE
The DJControl Inpulse T7 Premium weighs only 11 lbs, so you can carry it with the included bag anywhere you go. It also comes with retractable feet so you can run wires underneath and protect your controller from spilled drinks. No more calling you DJ Backpain, promise.
BETTER, SMOOTHER MOVEMENT
Each fader on the included and already installed Premium Fader Module on the DJControl Inpulse T7 Premium slides on 2 rails for better, smoother movement than the stock faders on the DJControl Inpulse T7. The 3 double-rail faders are built to last, so you can focus on your music, not your equipment.
MAKING BACKSPINS YOUR REALITY
Placed between the motorized jogwheel platter and the vinyl record, the included Scratch Slipmats insulate the records from platter vibrations and allow you to handle the disc without affecting the platter’s rotation. The DJControl Inpulse T7 Premium also come with standard slipmats, ideal for traditional mixing.
TOTAL COMFORT, IN TOTAL STYLE
Lighter than hardened plastic, the semi-rigid EVA (Ethylene Vinyl Acetate) bag has a black lining featuring the Hercules logo embroidered in white and red. The EVA creates a solid shell which is softer than hardened plastic and won’t break on impact. Your controller and its power cables will fit into a foam cavity, making it safe to carry everywhere your DJ career takes you.
ALL THE AUDIO CONNECTIONS YOU NEED
The DJControl Inpulse T7 Premium, powered by a DC converter and connected to your laptop via USB, provides crucial master outputs (2 x XLR + 2 x RCA) for connecting to professional speaker systems. To meet your various audio needs, it also offers dual headphone connectivity options (1/8" / 3.5 mm stereo mini-jack + 1/4" / 6.35 mm stereo jack).
The controller has been honored with Magnetic Mag's Editors Choice Award 2023, recognized as the best new DJ turntables of the year. This prestigious award highlights the publication's top picks in production, audio, and DJ gear categories.
For more details, visit: Magnetic Mag Editors Choice Awards 2023