Catalog Object Cloud
DELL

DELL Pro Plus P2725H computer monitor 68.6 cm (27") 1920 x 1080 pixels Full HD LCD Black

Product code:
DELL-P2725H
Brand:
DELL
Product family:
Pro Plus
Product name:
P2725H
GTIN (EAN/UPC):
5397184821749, 5715063417829, 5715063417850, 0884116468738, 884116468738
TCO Certified is the world’s most comprehensive sustainability certification for IT products, helping you make responsible product choices that drive the industry in a sustainable direction. Using TCO Certified also supports your organization’s efforts to reduce risk and take the next step in social and environmental responsibility.
D means that the product is rated in its category in terms of energy efficiency. The Energy Labeling system is based on EU Regulation 2017/1369/EU.
Bullet Points DELL Pro Plus P2725H computer monitor 68.6 cm (27") 1920 x 1080 pixels Full HD LCD Black:
  • 68.6cm (27") Full HD 1920 x 1080 LED IPS
  • 8ms, 16:9, 300cd/m², 1500:1
  • USB, VGA, HDMI, DisplayPort
Warranty:
3 Years Base Adv Ex
Long product name DELL Pro Plus P2725H computer monitor 68.6 cm (27") 1920 x 1080 pixels Full HD LCD Black:
68.6cm (27") Full HD 1920 x 1080 LED IPS, 16:9, 300cd/m², 16.7M, 8ms, 178°/178°, 1500:1
DELL Pro Plus P2725H computer monitor 68.6 cm (27") 1920 x 1080 pixels Full HD LCD Black:
Stay productive. Get enhanced visual comfort and seamless connectivity with this 27-in FHD monitor, certified by TÜV for 4-star eye comfort.
Disclaimer DELL Pro Plus P2725H computer monitor 68.6 cm (27") 1920 x 1080 pixels Full HD LCD Black $DELL-P2725H:
Actual configuration might differ from illustration
Product Carbon Footprint (PCF)
1. Dell calculates the Product Carbon Footprint using one of two methodologies, depending on the product: the Dell PCF calculator (GaBi version XXX, YYYY) or the Product Attribute to Impact Algorithm (PAIA, X.X.X, YYYY). The methodology used is indicated in the "Version of PCF tool used" column.
2. PAIA (Product Attribute Impact Algorithm) is a streamlined LCA tool developed by MIT ‘s Materials System Laboratory. PAIA estimates the product’s carbon footprint using limited system attributes of the product such as component dimension, screen size, system weight, and annual energy consumption.
3. Please note the emission estimate in this report is calculated using the mean value along with the standard deviation for that product model.
4. Use of default inputs (i.e. not primary data) and assumptions on location of use and other fields can introduce a standard deviation which must be taken into account while completing the calculations. For more information refer to the PCF pages on Dell.com.
5. For the PAIA PCF methodology, the transportation from assembly to customer includes the emissions generated during air, ocean and land transportation of finished or semi-finished Dell products between Dell facilities and between Dell facilities to customers.
6. For the Dell PCF calculator and methodology, the transportation phase the default delivery assumptions are 90% of transport happening by sea and 10% happening by air. Trucking distances don’t contribute as much to the PCF impact compared to more influential by sea or by air distances modes.
7. Please note, PAIA uses the ecoinvent Database (https://ecoinvent.org/the-ecoinvent-database/) whenever primary data is not made available for calculations.
8. For client and commercial end user computing products, minimum configurations were assumed for calculations. For Server and Storage products, typical configurations or ENERGY STAR (https://www.energystar.gov/products) configurations were used for calculations.
9. Use Phase emissions were calculated based on the location of use as "Europe" i.e. the Use Phase emissions are not specific to a single country / location.The Dell PCF Calculator also estimates Use Phase emissions for the U.S. and China, which are available in the PCF PDF documents on Dell.com.
10. The report provides the total emissions separated by the 4 lifecycle phases: manufacturing, transport, use, and end of life to understand the impact of each phase.
11. The Dell PCF Calculator lifetime usage assumption at the product family level is as follows: Desktop, Notebook - 5 years, Display - 6 years and Servers/Storage - 4 years.
12. For Displays, total product weight refers to the weight of the typical product configuration, including any cables and the power cord.
* Blanks indicate we do not have the corresponding metric calculated or data is currently unavailable for the specific product at this time.