Celly GHOSTSUPERMAGCH holder Passive holder Mobile phone/Smartphone Black
Product code:
GHOSTSUPERMAGCH
Brand:
Celly
Product name:
GHOSTSUPERMAGCH
GTIN (EAN/UPC):
8021735199182
Bullet Points Celly GHOSTSUPERMAGCH holder Passive holder Mobile phone/Smartphone Black:
- Car Passive holder
- Mobile device type: Mobile phone/Smartphone
- Car vent mount
- Built-in charger Wireless charging
- Black
Long product name Celly GHOSTSUPERMAGCH holder Passive holder Mobile phone/Smartphone Black:
MagSafe Car Holder, Plastic, 8 x 6 x 8.2 cm, Black
Celly GHOSTSUPERMAGCH holder Passive holder Mobile phone/Smartphone Black:
GHOSTSUPERMAGBK is a car mount compatible with the MagSafe magnetic alignment of the latest iPhone models, from 12 onwards. When you place your iPhone onto the holder, the circular magnet will automatically hook onto the device's magnetic module and lock it securely in place.
The air vent clip has been improved and equipped with a super resistant anti-fall system: the small hook in the final part of the clip hooks onto the fan fins making GHOSTSUPERMAGBK more performing in terms of stability and grip. The clip is also adjustable, so that the holder can be securely attached to the majority of air vents. The head has a 360° rotation to allow you to adjust the holder to the best angle.
The magnetic fixing system is specially designed to work with the latest iPhone models and is therefore completely safe and does not interfere with the smartphone.
Included in the box an additional metallic plate to increase the grip of the holder if you have a sporty driving or if you want to use the holder also with other smartphone models.
The air vent clip has been improved and equipped with a super resistant anti-fall system: the small hook in the final part of the clip hooks onto the fan fins making GHOSTSUPERMAGBK more performing in terms of stability and grip. The clip is also adjustable, so that the holder can be securely attached to the majority of air vents. The head has a 360° rotation to allow you to adjust the holder to the best angle.
The magnetic fixing system is specially designed to work with the latest iPhone models and is therefore completely safe and does not interfere with the smartphone.
Included in the box an additional metallic plate to increase the grip of the holder if you have a sporty driving or if you want to use the holder also with other smartphone models.