Hisense Built in 25 L microwave with grill. Inverter technology ensures even heating, while microwave + grill combines speed and crisp results. Auto programmes and defrost functions make everyday cooking simple.
Product code:
742528
Brand:
Hisense
Product name:
Built in 25 L microwave with grill. Inverter technology ensures even heating, while microwave + grill combines speed and crisp results. Auto programmes and defrost functions make everyday cooking simple.
GTIN (EAN/UPC):
3838782710162
Bullet Points Hisense Built in 25 L microwave with grill. Inverter technology ensures even heating, while microwave + grill combines speed and crisp results. Auto programmes and defrost functions make everyday cooking simple.:
- Built-in Grill microwave 25 L 900 W Black
- Grill 1200 W
- Defrost function
- Turntable 31.5 cm
- Touch Integrated clock Child lock
- Number of power levels: 5 Number of auto cooking programs: 15
Long product name Hisense Built in 25 L microwave with grill. Inverter technology ensures even heating, while microwave + grill combines speed and crisp results. Auto programmes and defrost functions make everyday cooking simple.:
Built in 25 L microwave with grill. Inverter technology ensures even heating, while microwave + grill combines speed and crisp results. Auto programmes and defrost functions make everyday cooking simple.
Hisense Built in 25 L microwave with grill. Inverter technology ensures even heating, while microwave + grill combines speed and crisp results. Auto programmes and defrost functions make everyday cooking simple.:
Aqua Cleaning
Fill a microwave safe glass or clay cup with tap water, place it in the oven, and activate the Aqua Clean program to clean the oven interior. The steam produced will soften any grime on the oven walls. Simply wipe down the oven with a moist cloth at the end of the program.
Auto Defrost
In order to keep the food in perfect condition after defrosting, it is important to thaw it efficiently. With defrost function the heat reaches the food evenly and simultaneously, with no need to manually lower the power. The quickest way to defrost.
Child Safety
The child safety lock provides you with additional piece of mind and the highest level of safety by preventing children from starting the oven inadvertently.
Clear Control
Keypads with larger touching pad fit nicely to the modern designed devices, with no space between the switches, thus eliminating the chance of dust accumulation. The control panel will alwyas be tidy and clean.
Crispy Grill
Experience the joy of achieving the perfect crust on your favorite dishes with the Crispy Grill feature. Harnessing the power of microwaves and grill, it allows for quick and efficient browning.
ECO Function
By activating the ECO Function, you can reduce standby power. When not in use, the LED display screen and clock will turn off and will help save energy. Function allows you to turn off clock, if you don't want to see it.
Grill Combo
Combine the benefits of microwaves and grills to discover totally new culinary dimensions. You'll be impressed by the quicker cooking of smaller pieces of meat, pizzas, and other meals that require precise frying and crisping.
Inverter Technology
With inverter technology, not simply reheating but also a new dimension of cooking is now possible. Microwaves with inverters allow continuous power output, as opposed to traditional technology, which produces lower power by cycling between 0% and 100% power. This guarantees that the food is evenly cooked during the cooking procedure.
LED Lighting
LED Lighting provides high-quality, energy-efficient illumination. It has a thirty-fold longer usable life than traditional light bulbs and saves up to ten times as much energy. White light allows to always properly see inside the oven.
Microwave Function
This oven is super useful because of its microwave function, which is used for fast reheating, defrosting, and cooking of food. You can now quickly defrost ready meals or reheat any leftovers.
Multiphase Cooking
You can cook in two stages by manually programming steps of the cooking process. For example, in step 1 you may opt for more microwaves than grill, in step 2 choose just grilling to achieve a final crust. When you activate this mode, the microwave oven automatically follows the steps so you don‘t have to do it manually.
Preset Programs
Automatic presets make it easier to cook certain foods like popcorn, chicken nuggets, pizza, and pasta. You only need to select the type of food and enter the weight, and the oven will adjust the cooking power and duration automatically. On top oven offers a plate warming function.
Quick Start
When you don't have time to wait for a hot supper use Quick Start, which allows for instant heating of food with a single touch. Just one press to quickly start a standard 30 second operation, and each next will increase the time.
Sound Control
The volume of acoustic signals can be adjusted in the microwave oven. while you need silence, such as while your kid is sleeping, you can operate your microwave oven without creating a sound; simply switch off the acoustic signals and turn them back on later.
Time & Weight Defrost
Defrost settings for this microwave includes 2 options - by time or weight. By using weight defrost, you simply chose the food catagory and enter the weight; the defrosting power and time will be adjusted automatically, preserving the original texture and flavor of the ingredients.
Fill a microwave safe glass or clay cup with tap water, place it in the oven, and activate the Aqua Clean program to clean the oven interior. The steam produced will soften any grime on the oven walls. Simply wipe down the oven with a moist cloth at the end of the program.
Auto Defrost
In order to keep the food in perfect condition after defrosting, it is important to thaw it efficiently. With defrost function the heat reaches the food evenly and simultaneously, with no need to manually lower the power. The quickest way to defrost.
Child Safety
The child safety lock provides you with additional piece of mind and the highest level of safety by preventing children from starting the oven inadvertently.
Clear Control
Keypads with larger touching pad fit nicely to the modern designed devices, with no space between the switches, thus eliminating the chance of dust accumulation. The control panel will alwyas be tidy and clean.
Crispy Grill
Experience the joy of achieving the perfect crust on your favorite dishes with the Crispy Grill feature. Harnessing the power of microwaves and grill, it allows for quick and efficient browning.
ECO Function
By activating the ECO Function, you can reduce standby power. When not in use, the LED display screen and clock will turn off and will help save energy. Function allows you to turn off clock, if you don't want to see it.
Grill Combo
Combine the benefits of microwaves and grills to discover totally new culinary dimensions. You'll be impressed by the quicker cooking of smaller pieces of meat, pizzas, and other meals that require precise frying and crisping.
Inverter Technology
With inverter technology, not simply reheating but also a new dimension of cooking is now possible. Microwaves with inverters allow continuous power output, as opposed to traditional technology, which produces lower power by cycling between 0% and 100% power. This guarantees that the food is evenly cooked during the cooking procedure.
LED Lighting
LED Lighting provides high-quality, energy-efficient illumination. It has a thirty-fold longer usable life than traditional light bulbs and saves up to ten times as much energy. White light allows to always properly see inside the oven.
Microwave Function
This oven is super useful because of its microwave function, which is used for fast reheating, defrosting, and cooking of food. You can now quickly defrost ready meals or reheat any leftovers.
Multiphase Cooking
You can cook in two stages by manually programming steps of the cooking process. For example, in step 1 you may opt for more microwaves than grill, in step 2 choose just grilling to achieve a final crust. When you activate this mode, the microwave oven automatically follows the steps so you don‘t have to do it manually.
Preset Programs
Automatic presets make it easier to cook certain foods like popcorn, chicken nuggets, pizza, and pasta. You only need to select the type of food and enter the weight, and the oven will adjust the cooking power and duration automatically. On top oven offers a plate warming function.
Quick Start
When you don't have time to wait for a hot supper use Quick Start, which allows for instant heating of food with a single touch. Just one press to quickly start a standard 30 second operation, and each next will increase the time.
Sound Control
The volume of acoustic signals can be adjusted in the microwave oven. while you need silence, such as while your kid is sleeping, you can operate your microwave oven without creating a sound; simply switch off the acoustic signals and turn them back on later.
Time & Weight Defrost
Defrost settings for this microwave includes 2 options - by time or weight. By using weight defrost, you simply chose the food catagory and enter the weight; the defrosting power and time will be adjusted automatically, preserving the original texture and flavor of the ingredients.